Rebulid VSDK kernel modules error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Rebulid VSDK kernel modules error

2,276 Views
6905324
Contributor II

Hi,

I want to rebulid kernel like csi.o, and while reading VisionSDK_S32V2_RTM_1_3_0 user guide. Some questions occurred at 3.3.1 and 3.3.2. 

3.3.1General Preparation
o export LINUX_S32V234_DIR=/linux/sources/directory/for/s32v234/
       optional, only for s32v234 Linux build
       Path to the Linux sources (same kernel as is running on the board)
o export PATH=/path/to/your/compiler/binaries:$PATH
        Path to the compiler binaries

I can't find "linux sources" directory in VisionSDK_S32V2_RTM_1_3_0 folders. And if I try to run "make allsub" on Windows via msys32 in "VisionSDK_S32V2_RTM_1_3_0\s32v234_sdk\libs\isp\csi\kernel\build-v234ce-gnu-linux-d", 

I got this: Makefile:81: *** Please define LINUX_S32V234_DIR pointing to kernel directory 

@bpe

 

Labels (2)
0 Kudos
Reply
2 Replies

2,197 Views
bpe
NXP Employee
NXP Employee

Please be aware, that support to S32V234 Vision subsystem modules is done only
via tickets. This Community is not appropriate for questions of this kind. I
will contact you by e-Mail with respect to this issue, for future requests,
please:

1. Register yourself on NXP Website with your corporate e-Mail.

2.  Use tickets to submit questions.

 
Have a great day,
Platon

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

2,197 Views
6905324
Contributor II

Thanks bpe!

I've created my questions in support system, and how can I get more information or how to figure it out?

0 Kudos
Reply