PIT interrupt code is disabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PIT interrupt code is disabled

Jump to solution
2,377 Views
Dev15
Contributor III

Hi Team,

 

I have configured PIT0 and PIT1. The ISR is not getting interrupted as expected as the code is disabled in "Pit_Ip.c" file.

Please find the attached screen shot for reference and help to resolve the same.

RTD 3.0.0 version is used

Dev15_0-1710786343442.pngDev15_0-1710786343442.pngt

 

Dev15_1-1710786369983.pngDev15_1-1710786369983.png

 

Dev15_2-1710786505332.pngDev15_2-1710786505332.png

 

 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,289 Views
Dev15
Contributor III

@Senlent , Thank you. It is working fine now.

View solution in original post

0 Kudos
Reply
2 Replies
2,350 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Dev15

I did some tests on the routines provided by the IDE.

Attached is the project I modified. I hope it will be helpful to you.

0 Kudos
Reply
2,290 Views
Dev15
Contributor III

@Senlent , Thank you. It is working fine now.

0 Kudos
Reply