PIT interrupt code is disabled

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PIT interrupt code is disabled

ソリューションへジャンプ
2,413件の閲覧回数
Dev15
Contributor III

Hi Team,

 

I have configured PIT0 and PIT1. The ISR is not getting interrupted as expected as the code is disabled in "Pit_Ip.c" file.

Please find the attached screen shot for reference and help to resolve the same.

RTD 3.0.0 version is used

Dev15_0-1710786343442.pngDev15_0-1710786343442.pngt

 

Dev15_1-1710786369983.pngDev15_1-1710786369983.png

 

Dev15_2-1710786505332.pngDev15_2-1710786505332.png

 

 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,325件の閲覧回数
Dev15
Contributor III

@Senlent , Thank you. It is working fine now.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,386件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Dev15

I did some tests on the routines provided by the IDE.

Attached is the project I modified. I hope it will be helpful to you.

0 件の賞賛
返信
2,326件の閲覧回数
Dev15
Contributor III

@Senlent , Thank you. It is working fine now.

0 件の賞賛
返信