Overview of SDK Versions?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Overview of SDK Versions?

ソリューションへジャンプ
1,174件の閲覧回数
tsweaver
Contributor II

As I understand it, 3.5 is the latest version of S32DS and 3.0.3 is the latest SDK.  I read in another post that there is no plan to integrate SDK 3.0.3 into DS 3.5.  Can someone please explain why that is?  What currently is the latest and greatest combination of DS and SDK that is ready for production use? I've not been able to find an overview of different versions and inter-dependencies.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,161件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for the inconvenience we bring you! 
S32K1 SDK RTM 4.0.3 is the latest SDK and it was developed in S32DS v3.4.
Please check the release note of S32K1 SDK to see which S32DS is developed with.

After that(4.0.3), the S32K1 SDK will no longer be updated, but will be replaced by S32K1 RTD. Correspondingly, the latest S32K1_S32M24X Real Time Drivers AUTOSAR 4.4 & R21-11 Version 2.0.0 is developed based on S32DS v3.5. Since S32K1 RTD was released relatively recently, there is relatively little relevant information in the community.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

1 返信
1,162件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for the inconvenience we bring you! 
S32K1 SDK RTM 4.0.3 is the latest SDK and it was developed in S32DS v3.4.
Please check the release note of S32K1 SDK to see which S32DS is developed with.

After that(4.0.3), the S32K1 SDK will no longer be updated, but will be replaced by S32K1 RTD. Correspondingly, the latest S32K1_S32M24X Real Time Drivers AUTOSAR 4.4 & R21-11 Version 2.0.0 is developed based on S32DS v3.5. Since S32K1 RTD was released relatively recently, there is relatively little relevant information in the community.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------