Offline Automotive Software Package Manager

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Offline Automotive Software Package Manager

ソリューションへジャンプ
2,614件の閲覧回数
ClemensGruenberger
Contributor I

Is there a way to get the content as offline Installer or package?
I need some software packages for the S32G2 and it's manuals available from "Automotive Software Package Manager"


Our IT restrictions do not easily allow us to use dynamic installers needing admin-privileges.
I went through the process of getting the privileges temporarily, but the downloader can't connect to the NXP server... 

So the most convenient way for me would be to get the desired content as a direct http or ftp download.

If not possible, which are the ports needed to be allowed to use downloader?

 

Kind Regards
Clemens

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,602件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

There is an alternative that could help you to obtain the needed packages for your development. Below will be some steps that should lead you to this page:

- Sign in to your NXP account (link to NXP site: NXP® Semiconductors Official Site | NXP Semiconductors)
- Click on "My NXP Account" (top-right) and click on "Software Licensing and Support" under the "Licensing" section within the window it opens.
- This will redirect you to another page. In this new page, select the option "View Accounts" under the "Software accounts" section.
- This will again redirect you to another page. On this page, you should see different sections with the "Automotive SW" words on it. The below steps will be for downloading the Real-Time Drivers for M7.
- Click on the "Automotive SW – S32G Standard Software". Next, click on the "Automotive SW - S32G - Real Time Drivers (RTD) (Cortex-M7)". Next, click on the "S32G Real_Time Drivers 4_4 Version 3_0_3".
- Once you accept the Terms and conditions, the package needed is the one with the "updatesite" word in it (should be "SW32G_RTD_4.4_3.0.3_DS_updatesite_D2206.zip")

This should download the updatesite needed for S32DS v3.4 to install the RTD.

Please, let us know if this information was helpful or not. 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,603件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

There is an alternative that could help you to obtain the needed packages for your development. Below will be some steps that should lead you to this page:

- Sign in to your NXP account (link to NXP site: NXP® Semiconductors Official Site | NXP Semiconductors)
- Click on "My NXP Account" (top-right) and click on "Software Licensing and Support" under the "Licensing" section within the window it opens.
- This will redirect you to another page. In this new page, select the option "View Accounts" under the "Software accounts" section.
- This will again redirect you to another page. On this page, you should see different sections with the "Automotive SW" words on it. The below steps will be for downloading the Real-Time Drivers for M7.
- Click on the "Automotive SW – S32G Standard Software". Next, click on the "Automotive SW - S32G - Real Time Drivers (RTD) (Cortex-M7)". Next, click on the "S32G Real_Time Drivers 4_4 Version 3_0_3".
- Once you accept the Terms and conditions, the package needed is the one with the "updatesite" word in it (should be "SW32G_RTD_4.4_3.0.3_DS_updatesite_D2206.zip")

This should download the updatesite needed for S32DS v3.4 to install the RTD.

Please, let us know if this information was helpful or not. 

0 件の賞賛
返信