Offline Automotive Software Package Manager

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Offline Automotive Software Package Manager

Jump to solution
2,646 Views
ClemensGruenberger
Contributor I

Is there a way to get the content as offline Installer or package?
I need some software packages for the S32G2 and it's manuals available from "Automotive Software Package Manager"


Our IT restrictions do not easily allow us to use dynamic installers needing admin-privileges.
I went through the process of getting the privileges temporarily, but the downloader can't connect to the NXP server... 

So the most convenient way for me would be to get the desired content as a direct http or ftp download.

If not possible, which are the ports needed to be allowed to use downloader?

 

Kind Regards
Clemens

 

Labels (1)
0 Kudos
Reply
1 Solution
2,634 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

There is an alternative that could help you to obtain the needed packages for your development. Below will be some steps that should lead you to this page:

- Sign in to your NXP account (link to NXP site: NXP® Semiconductors Official Site | NXP Semiconductors)
- Click on "My NXP Account" (top-right) and click on "Software Licensing and Support" under the "Licensing" section within the window it opens.
- This will redirect you to another page. In this new page, select the option "View Accounts" under the "Software accounts" section.
- This will again redirect you to another page. On this page, you should see different sections with the "Automotive SW" words on it. The below steps will be for downloading the Real-Time Drivers for M7.
- Click on the "Automotive SW – S32G Standard Software". Next, click on the "Automotive SW - S32G - Real Time Drivers (RTD) (Cortex-M7)". Next, click on the "S32G Real_Time Drivers 4_4 Version 3_0_3".
- Once you accept the Terms and conditions, the package needed is the one with the "updatesite" word in it (should be "SW32G_RTD_4.4_3.0.3_DS_updatesite_D2206.zip")

This should download the updatesite needed for S32DS v3.4 to install the RTD.

Please, let us know if this information was helpful or not. 

View solution in original post

0 Kudos
Reply
1 Reply
2,635 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

There is an alternative that could help you to obtain the needed packages for your development. Below will be some steps that should lead you to this page:

- Sign in to your NXP account (link to NXP site: NXP® Semiconductors Official Site | NXP Semiconductors)
- Click on "My NXP Account" (top-right) and click on "Software Licensing and Support" under the "Licensing" section within the window it opens.
- This will redirect you to another page. In this new page, select the option "View Accounts" under the "Software accounts" section.
- This will again redirect you to another page. On this page, you should see different sections with the "Automotive SW" words on it. The below steps will be for downloading the Real-Time Drivers for M7.
- Click on the "Automotive SW – S32G Standard Software". Next, click on the "Automotive SW - S32G - Real Time Drivers (RTD) (Cortex-M7)". Next, click on the "S32G Real_Time Drivers 4_4 Version 3_0_3".
- Once you accept the Terms and conditions, the package needed is the one with the "updatesite" word in it (should be "SW32G_RTD_4.4_3.0.3_DS_updatesite_D2206.zip")

This should download the updatesite needed for S32DS v3.4 to install the RTD.

Please, let us know if this information was helpful or not. 

0 Kudos
Reply