MPC57XX EAR SDK, LIN Master-Slave Example Project?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC57XX EAR SDK, LIN Master-Slave Example Project?

5,843件の閲覧回数
eyupozer
Contributor III

Hi,

Is there any LINFlex LIN Master-Slave example or demo projects for S32DS, MPC57XX EAR SDK V0.8.1?

I've got an MPC574XG evaluation board with MPC5746C MCU. I want to use LIN0 and LIN1 port but there is no example configuration project for LIN Flex Master-Slave communication?

Thanks

タグ(4)
7 返答(返信)

5,646件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I received confirmation from development team that LIN support for MPC5748G is not planned.

Sorry for any inconvenience.

Regards,

Martin

0 件の賞賛
返信

5,637件の閲覧回数
bwp530
Contributor IV

hi @martin_kovar 

Do you mean that there is no lin master in SDK? I'm using the MPC5748G RTM3.0, and I don't find any lin master in components library.

0 件の賞賛
返信

5,646件の閲覧回数
eyupozer
Contributor III

Thanks Martin for the quick support.

0 件の賞賛
返信

5,646件の閲覧回数
李月鑫
Contributor I

Hello:

     I am currently planning to do the LIN function development of 5748G, but I have encountered the same problem as you. I did not find relevant samples in the SDK. How did you solve it?

Best Regards

0 件の賞賛
返信

5,646件の閲覧回数
eyupozer
Contributor III

Hello,
I did not find any demo project, I've solved this problem without SDK.

0 件の賞賛
返信

4,864件の閲覧回数
minghu_du
Contributor III

Hello eyupozer,

I am also trying to configure LINFlexD to LIN mode, could you please share your code with me?

Best Regards,

0 件の賞賛
返信

5,646件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

unfortunately, there is no example for LINFlex in SDK available at all. I will ask SDK development team, if there is any plan to create one (but for SDK RTM 2.0.0) and I will let you know.

Regards,

Martin