MPC5748G- UART_PAL not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5748G- UART_PAL not working

1,413件の閲覧回数
logan_r
Contributor I

Hi,

I have changed clock to 24MHz, and trying to enable uart_pal. LINFlexD_2 is used in the given example uart_pal_mpc5748g, Where I have configured with LINFlexD_7 instead of LINFlexD_2.

But it is not working. Kindly do support.

 

Regards,

Logan 

0 件の賞賛
返信
2 返答(返信)

1,379件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I don't have a board with 24MHz crystal, so I can't test your project directly without changes. What is not working exactly? If you use an oscilloscope, is anything send out? When you debug the code, what can you see?

Regards,

Lukas

 

0 件の賞賛
返信

1,392件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @logan_r ,

As this relates to usage of the S32 SDK, we have relocated the post to be addressed by the experts for S32 SDK.

Mike

0 件の賞賛
返信