MPC5748G- UART_PAL not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G- UART_PAL not working

1,412 Views
logan_r
Contributor I

Hi,

I have changed clock to 24MHz, and trying to enable uart_pal. LINFlexD_2 is used in the given example uart_pal_mpc5748g, Where I have configured with LINFlexD_7 instead of LINFlexD_2.

But it is not working. Kindly do support.

 

Regards,

Logan 

0 Kudos
Reply
2 Replies

1,378 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I don't have a board with 24MHz crystal, so I can't test your project directly without changes. What is not working exactly? If you use an oscilloscope, is anything send out? When you debug the code, what can you see?

Regards,

Lukas

 

0 Kudos
Reply

1,391 Views
mikedoidge
NXP Employee
NXP Employee

Hello @logan_r ,

As this relates to usage of the S32 SDK, we have relocated the post to be addressed by the experts for S32 SDK.

Mike

0 Kudos
Reply