MPC5744P DEVKIT Using S32 SDK 0.9.0 BETA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MPC5744P DEVKIT Using S32 SDK 0.9.0 BETA

跳至解决方案
9,307 次查看
chuluezhong
Contributor II

I am trying to test the FlexCAN module using the S32 SDK 0.9.0 BETA for the MPC5744P. I have tried loading the example code, which on reception of a CAN message toggles the DEVKIT LEDs and also sends CAN messages when the switches are pressed. I am using a Vector VN1610 CAN-to-USB to communicate with the board when running, however, I seem to not be able to receive or send data to the board this way. On debug, I see that the program is stuck in the loop

while (FLEXCAN_DRV_GetTransferStatus(INST_CANCOM1, RX_MAILBOX) == STATUS_BUSY) { }

I have also monitored the signals from the CAN ports on the DEVKIT as well as the Vector VN1610 and I can read signals on the scope so I am unsure why the the transfer status cannot 'finish' i.e. the loop is infinite.

i have attached my set-up as well as the tests I have made on the oscilloscope.

0 项奖励
回复
1 解答
8,783 次查看
stanish
NXP Employee
NXP Employee

Hi,

I'd recommend to add terminating resistor 120 ohm between CAN_H and  CAN_L terminals or populate SMD resistor 120 Ohm - R38 pads

pastedImage_1.pngAlso please make sure you setup the CAN bus correctly on the PC side:

500kbps, 85% sampling point

Hope it helps.

Stan 

在原帖中查看解决方案

0 项奖励
回复
5 回复数
8,783 次查看
vernonhawes
Contributor I

Hi Chulue Zhong, Could you please share the example code which you used with the DEVKIT to transmit and receive CAN signals on the CAN0 port?

The example included with the S32 Design studio for MPC5744P DEVKIT sends CAN messages on CAN2 and I'm not sure how to monitor these using a Vector CAN case HW and Vector CANoe.

Thanks in advance.

0 项奖励
回复
8,783 次查看
chuluezhong
Contributor II

The way I set up CAN was to use Processor Expert with the S32 SDK, which is an addon you can get from the S32 download page I believe. Then you can choose which FlexCAN module to use in a graphical interface and then add functionality by dragging and dropping code. Hence the final code set-up (FlexCAN only) for me was

in "main()":

    // FlexCAN message struct for sending
    flexcan_msgbuff_t send_buff;
    send_buff.data[0] = 0;
    send_buff.data[1] = 0xFF;
    send_buff.data[2] = 0;
    send_buff.data[3] = 0xFF;
    send_buff.data[4] = 0;
    send_buff.data[5] = 0xFF;
    send_buff.data[6] = 0;
    send_buff.data[7] = 0xFF;
    send_buff.dataLen = 8; // data length
    send_buff.msgId = 1; // Message ID

    // FlexCAN Data Info
    flexcan_data_info_t txInfo = {
            .data_length = 8,
            .is_remote = 0,
            .msg_id_type =     FLEXCAN_MSG_ID_STD,
    };

   // Initialize FlexCAN module
    FLEXCAN_DRV_Init(INST_CANCOM1, &canCom1_State, &canCom1_InitConfig0);

    // Configure Tx Message Buffer 0 to send CAN message
    FLEXCAN_DRV_ConfigTxMb(INST_CANCOM1, 0, &txInfo,  send_buff.msgId);

    // Send the message
    FLEXCAN_DRV_Send(INST_CANCOM1, 0, &txInfo, send_buff.msgId, &(send_buff.data));

    while(1)
    {
        // Wait for transfer to complete
        while (FLEXCAN_DRV_GetTransferStatus(INST_CANCOM1, 0) == STATUS_BUSY) {
            //FLEXCAN_DRV_Send(INST_CANCOM1, 0, &txInfo, send_buff.msgId, &(send_buff.data));
            counter++;
        }
    }

If you don't use the S32 SDK I think you can just replace CAN2 with CAN0 in the example code you saw, but you probably need to pay attention to the peripheral clocking for CAN0. On the DEVKIT, only CAN0 is connected to a proper CAN transceiver (MC33901WEF, see above) so with minimal set-up you would just need a 120-ohm resistor and some wires to connect to the Vector CAN peripherals.

0 项奖励
回复
8,784 次查看
stanish
NXP Employee
NXP Employee

Hi,

I'd recommend to add terminating resistor 120 ohm between CAN_H and  CAN_L terminals or populate SMD resistor 120 Ohm - R38 pads

pastedImage_1.pngAlso please make sure you setup the CAN bus correctly on the PC side:

500kbps, 85% sampling point

Hope it helps.

Stan 

0 项奖励
回复
8,783 次查看
chuluezhong
Contributor II

I do have an additional follow-up question, however. Are the values 500kbps and 85% sampling point dependent on the CAN transceiver (MC33901WEF) in the case of the DEVKIT? Also, the default sampling point was 87.5% actually, which worked.

0 项奖励
回复
8,783 次查看
chuluezhong
Contributor II

Thanks very much, I now have the example code working. I thought initially that this resistor was already on the board.

0 项奖励
回复