LPI2C and FlexIO_I2S Clock Initialization API

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

LPI2C and FlexIO_I2S Clock Initialization API

跳至解决方案
1,050 次查看
MohitManvar
Contributor III

Hello,

Board: S32K142 Eval board

In sample codes of LPI2C and FexIO_I2S, the APIs used for initializing clock are different.

What is the significance for both APIs and when can each of them be used?

The issue we are facing is, when we are trying to combine both peripheral  configurations (i2c and i2s), it is now working. No clocks generated for i2c (scl) or i2s (sclk)

Could this be because of the use of different APIs for Clock init?

Or is there any other configuration impacting the functionality

Sample code snippets below:

MohitManvar_0-1692710812005.png

 

标签 (1)
0 项奖励
回复
1 解答
1,027 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for the inconvenience we bring you!

The CLOCK_SYS_* API was deprecated
CLOCK_SYS_Init();
CLOCK_SYS_UpdateConfiguration(); 
can be replaced with:
CLOCK_DRV_Init(&clockMan1_InitConfig0);

Similar topics are discussed in SDK problem in S32 Design Studio for ARM 2.2


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,028 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Sorry for the inconvenience we bring you!

The CLOCK_SYS_* API was deprecated
CLOCK_SYS_Init();
CLOCK_SYS_UpdateConfiguration(); 
can be replaced with:
CLOCK_DRV_Init(&clockMan1_InitConfig0);

Similar topics are discussed in SDK problem in S32 Design Studio for ARM 2.2


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复