LIN Middleware stack missing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LIN Middleware stack missing

ソリューションへジャンプ
8,777件の閲覧回数
SivaB
Contributor III

LIN middleware stack is available on when selecting SDK S32SDK_S32K1XX_RTM_4.0.1 & tool chain version GCC 6.3.

LIN middleware stack is missing on PLATFORMSDK_S32K1_2022_02_S32K144_M4F_1.0.1 () & tool chain version GCC 9.2

How to add LIN stack and LDF file for SDK SW32K1_RTD_4_4_1_0_1_D2202.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
8,748件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

for SDK SW32K1_RTD_4_4_1_0_1_D2202 you would need select right LIN stack version

 

2023-05-16_14-35-07.png

after succesful intallation you shoul dsee stack added in RTD folder

PetrS_1-1684241058071.png

and on example created in RTD 1.0.1 you will have option to add this stack in Middleware section

PetrS_2-1684241143562.png

Or you can create new example from a demo one

PetrS_3-1684241279784.png

BR, Petr

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
8,760件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

you need to download stack from S32K1 referenced SW and add it to the S32DS;
https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K1-REFSW-D

PetrS_0-1684235972430.png

 

BR, Petr

0 件の賞賛
返信
8,749件の閲覧回数
SivaB
Contributor III

I have installed the LINSTACK S32K1 1.0.2, but driver is not available on components list.

0 件の賞賛
返信
8,749件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

for SDK SW32K1_RTD_4_4_1_0_1_D2202 you would need select right LIN stack version

 

2023-05-16_14-35-07.png

after succesful intallation you shoul dsee stack added in RTD folder

PetrS_1-1684241058071.png

and on example created in RTD 1.0.1 you will have option to add this stack in Middleware section

PetrS_2-1684241143562.png

Or you can create new example from a demo one

PetrS_3-1684241279784.png

BR, Petr

0 件の賞賛
返信
8,738件の閲覧回数
SivaB
Contributor III
Hello BR, Petr,
Thanks for your support, now middleware LIN components available on SDK SW32K1_RTD_4_4_1_0_1_D2202
0 件の賞賛
返信