ISELED SDK for S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISELED SDK for S32DS

2,184 Views
victor_song_171
Contributor III

I installed S32K1_ISELED_RTM_3.0.0 in the directory of S32SDK_S32K1xx_RTM_3.0.0 . Then create the project from Example , and the error report like below:

QQ浏览器截图20190504214550.png

and the component like below:

pastedImage_2.png

What should do ? thanks for any assistance.

PS: Just installed "Hooks for S32DS S32K1xx RTM SDK 3.0.0" and "S32 DS S32K1xx RTM SDK 3.0.0" and "S32 DS S32K1xx RTM SDK 3.0.0 path"

0 Kudos
Reply
2 Replies

1,913 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

please update your S32DS Instalation - https://community.nxp.com/docs/DOC-341068

With latest updates can be iseled example build without any issue. 

Hope it helps. 

Jiri 

0 Kudos
Reply

1,913 Views
victor_song_171
Contributor III

It‘s worked,and thanks for assistance.

Another question: the document say : "after 10000 commands , all ISELED function will return DGIED_EVALUATION_OVER......so digLED_Init_Init_Interface must be called". when I called function digLED_Init_Interface(), it will cast 1 second that the led can not do anything. Is there any other method to reinitialized the solve this problem in shorter time ?

0 Kudos
Reply