Hi,
The flexCan demo use polling to recieve data, i want to use flexCan interrupt.
I have made flexCan0 IRQ enable, and defined callback function.



According to (https://community.nxp.com/t5/S32K/Flexcan-interrupt-mode/m-p/785362), define callback function formit (See attachment).
But, it is not working normally. The first time can enter this function, second and others not enter IRQ function.
On debug:
TX mailbox is MB0, RX mailbox is MB1.
The first time, execute FlexCAN_Ip_Send(), Register IFLAG1 BIT0 and BIT1 is '1', transmit interrupt and reciver interrupt trigger(transmit interrupt not enable); after recieve interrupt callback, BIT1 clear.

then with debug tools, force to clear BIT0.

Second time, execute FlexCAN_Ip_Send(), Register IFLAG1 BIT0 and BIT1 no change. It seem abnormal.