Failed to read memory @ address 0x00000000

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Failed to read memory @ address 0x00000000

跳至解决方案
7,770 次查看
longli
Contributor I

Hi,

When I try to run debug mode, the consoles reports the following errors. I use the sample codes(LPUART_s32k144) in SDK and my device is s32k144(64pins). while I found the sample codes is for s32k44 100pins.  The same codes I can flash or run debug on your provided EVB.

How can I set the 64pins in NXP IDE?

what should I do to solve the fowllowing error?

Starting target CPU...

Reading all registers

WARNING: Failed to read memory @ address 0x00000000

Removing breakpoint @ address 0x000004C0, Size = 2

WARNING: Could not remove breakpoint @ address 0x000004C0

ERROR: Failed to set breakpoint at 0x000004C0

WARNING: Failed to read memory @ address 0x00000000

标签 (1)
标记 (3)
0 项奖励
回复
1 解答
6,816 次查看
razva_tilimpea
NXP Employee
NXP Employee
2 回复数
6,817 次查看
razva_tilimpea
NXP Employee
NXP Employee
3,871 次查看
Lita
Contributor II
The ide I am using is S32DS.3.5 and no Components Library is found.how do i?
0 项奖励
回复