Hi,
When I try to run debug mode, the consoles reports the following errors. I use the sample codes(LPUART_s32k144) in SDK and my device is s32k144(64pins). while I found the sample codes is for s32k44 100pins. The same codes I can flash or run debug on your provided EVB.
How can I set the 64pins in NXP IDE?
what should I do to solve the fowllowing error?
Starting target CPU...
Reading all registers
WARNING: Failed to read memory @ address 0x00000000
Removing breakpoint @ address 0x000004C0, Size = 2
WARNING: Could not remove breakpoint @ address 0x000004C0
ERROR: Failed to set breakpoint at 0x000004C0
WARNING: Failed to read memory @ address 0x00000000
已解决! 转到解答。
Hi,
Please check these 2 posts:
HOWTO: Change the CPU Derivative in an SDK-Based Application Project
https://community.nxp.com/docs/DOC-334936
Best regards,
Razvan
Hi,
Please check these 2 posts:
HOWTO: Change the CPU Derivative in an SDK-Based Application Project
https://community.nxp.com/docs/DOC-334936
Best regards,
Razvan