External Interrupt not detected in MPC5748G -SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

External Interrupt not detected in MPC5748G -SDK

1,280 次查看
kpdeshpande08
Contributor I

Hi,

I am writing an SDK application in S32Design Stodio for power architecture where I want an external interrupt on pin PA6. I have pulled up the pin and want to detect a falling edge on the pin so I am giving a low signal from GND on J4 on the MPC5748G development board. But my ISR doesn't get hit. I have checked the embSysRegisters in which the corresponding SUIL2-ISR flag is not set and I am also not able to configure SIUL2-MSCR1 for my external Interrupt1. I am attaching my zipped project.

标签 (1)
0 项奖励
回复
1 回复

1,153 次查看
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I can recommend to use the latest SDK driver.

Please refer to example posted here

https://community.nxp.com/docs/DOC-343728

Hope it helps.

BR, Petr

0 项奖励
回复