Error compiling APEX2 application using a graph

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error compiling APEX2 application using a graph

1,846 次查看
jorge_barrio
Contributor I

I am new on using the development board S32V234.

I am using VisionSDK_S32V2_RTM_1_4_1 to generate and compile my projects. I am following the documentation provided to generate a simple graph which resizes a simple image. I also tried to compile some of the simple examples provided such as Apex2_Add and Apex2_fast9. Unfortunately I am not able to compile successfully any of these projects either.

VisionSDK is installed and running in a Ubuntu 18.04 operating system.

The error I am getting is always related to the graph model. It seems like it is not generating the header file of the main module of the graph. For the Add example is missing the ADD.hpp file, which is nowhere. I wondering if there is some missing configuration parameter which is preventing  to fully compile the graph successfully.

Attached you can find an screen shot with the error reported. I would really appreciate if somebody could help me with this problem.

Please let me know if you need more information to find out the problem.

Much appreciated!

标记 (1)
0 项奖励
回复
0 回复数