FTM input capture and PWM with Processor Expert

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FTM input capture and PWM with Processor Expert

跳至解决方案
3,142 次查看
EE_CW
Contributor III

Hello together

I tried to use the FTM5 for generating a PWM Signal on Channel 0 and measure a Signal with Input Capture on Channel 1.

For this I added a ftm PWM component and a ftm IC component.

The problem is, that each FLEX Timer can only be assigned to one component. But If a PWM component has been choosen, only PWM can be configured within this component. The same problem with the input capture component.

So how can I realize this with processor expert?

s32_ftm.PNG

Thanky for your answers

Regards

Mario

标记 (3)
0 项奖励
回复
1 解答
2,948 次查看
razva_tilimpea
NXP Employee
NXP Employee

Hi Mario,

Exactly, the hardware doesn't have this type of restriction. So, you can do this use-case on your own.

Please check carefully this chapter"45.5.3.4 Counter reset".

If you want to accelerate your development I think you can keep one of the drivers PWM or OC and implement the other one with registers access to match your requirements. In this case production ready qualification will be affected.

Best regards,

Razvan

在原帖中查看解决方案

3 回复数
2,948 次查看
razva_tilimpea
NXP Employee
NXP Employee

Hi,

This is a limitation added in SDK because FTM have only one counter and if IC and PWM or other possible combination are used the counter can be reset and change the behavior of the application. For example period measurement can be affected if duty is update with immediate update.

Best regards,

Razvan

2,948 次查看
EE_CW
Contributor III

Hi Razvan

Thanks for your answer.

So that means, that with the Processor Expert it will be not possible.

But it is possible if I do not use the SDK, right?

Regards

Mario

0 项奖励
回复
2,949 次查看
razva_tilimpea
NXP Employee
NXP Employee

Hi Mario,

Exactly, the hardware doesn't have this type of restriction. So, you can do this use-case on your own.

Please check carefully this chapter"45.5.3.4 Counter reset".

If you want to accelerate your development I think you can keep one of the drivers PWM or OC and implement the other one with registers access to match your requirements. In this case production ready qualification will be affected.

Best regards,

Razvan