Can't find Interrupt manger component in SDK 4.0.2 RTM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't find Interrupt manger component in SDK 4.0.2 RTM

1,304 次查看
samcs
Contributor II

Hi , I opened an project on SDK 0.8.4 EAR, there is a component in PE, 

samcs_0-1646175698252.png

 

I try to re-config the project on SDK 4.0.2 RTM, but i can't find the Interrupt_manager , not in Drivers, nor in PAL.

How can we handle the interrupt manager in SDK 4.0.2 RTM?

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,296 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi samcs,

You can find Interrupt Manager (Interrupt): C:\NXP\S32DS.3.4\S32DS\software\S32SDK_S32K1XX_RTM_4.0.2\doc\Start_here

Interrupt Manager (Interrupt).png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复