CSEc key load result

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CSEc key load result

2,284 Views
yqs77
Contributor II

As I known, the CSEc key will be loaded in the format of M1, M2, M3, and the M4, M5 are used to check the result of key load. It is safe for that the calculation is irreversible, but I want to know that after loading the key to CSEc slot, whether the key is decrypted or still stored as the format of M1 to M5?

Labels (1)
0 Kudos
Reply
3 Replies

2,273 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it follows SHE specification:

lukaszadrapa_0-1655962241999.png

 Regards,

Lukas

0 Kudos
Reply

2,228 Views
yqs77
Contributor II

Thanks for the reply. Refer to the attachment, I will suppose that when the key like BOOT_MAC_KEY loaded to slot, it will be encrypted with the AES in ECB mode. And when it used like BOOT_MAC calculation, it is still read in AES encrypted form. Am I correct?

0 Kudos
Reply

2,185 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm sorry for delayed response.

From user's point of view, this is completely hidden to user. A user can use the keys or BOOT_MAC as needed and knowledge of these background operations is not needed. It follows SHE specification to ensure the keys / BOOT_MAC are protected as required. We can't share more details.

Regards,

Lukas

0 Kudos
Reply