APEX_CV:Cannot find input image

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

APEX_CV:Cannot find input image

Jump to solution
2,671 Views
liujinbao
Contributor II

hello,

   When I execute the program: apex_downsample_upsample_cv, the program outputs:

Cannot find input image data/common/in_gray_256x256.png.

2.png

   Other routines that need to open the image are the same result.

1.png

   The BSP version I am using is VisionSDK_S32V2_RTM_1_3_0_img_yocto

pastedImage_1.png

 The version of visionSDK I am using is  VisionSDK_S32V2_RTM_1_3_0_HF1

 The board model I am using is SBC-S32V234.

 

SBC-S32V234

SBC-S32V234

Tags (4)
0 Kudos
Reply
1 Solution
2,572 Views
liujinbao
Contributor II

hello,

   

  The data folder path is as follows:

3.png

The path in the source code is represented as data/common/in_grey_256x256.png,as shown below:

8.png

I copied the data/common/in_grey_256x256.png  to the development board, and the same path as the apex_downsample_upsample_cv.elf file.Program execution succeeded.

The test process is as follows: 

7.png

Thank you very much!!!

View solution in original post

0 Kudos
Reply
2 Replies
2,572 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you copy data folder (by default located in VSDK folder - c:\NXP\VisionSDK_S32V2_RTM_1_3_0\s32v234_sdk\demos\data ) next to your example executable? 

Jiri

0 Kudos
Reply
2,573 Views
liujinbao
Contributor II

hello,

   

  The data folder path is as follows:

3.png

The path in the source code is represented as data/common/in_grey_256x256.png,as shown below:

8.png

I copied the data/common/in_grey_256x256.png  to the development board, and the same path as the apex_downsample_upsample_cv.elf file.Program execution succeeded.

The test process is as follows: 

7.png

Thank you very much!!!

0 Kudos
Reply