ADC Data destination - S32K3xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Data destination - S32K3xx

ソリューションへジャンプ
1,845件の閲覧回数
MVR
Contributor V

When I define the ADC data destination to FIFO_1, if I'm using DMA, the watermark notification will be notify when the FIFO is full and in this moment the data will be already in the DMA buffer?

Thanks,

MVR

ラベル(1)
0 件の賞賛
返信
1 解決策
1,807件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, you can use both.You may specify at which FIFO entry DMA request is triggered.

davidtosenovjan_0-1661858975422.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,837件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you please explain your question more in detail? Thanks

0 件の賞賛
返信
1,815件の閲覧回数
MVR
Contributor V

I'm sorry, improving my question:

I would like to understand if it is possible to work FIFO_1 and DMA together or I need to choose only one of both...

Now I'm using only FIFO and all works, there is a notification when finish the ADC conversion, but in the future I will work with DMA, and I would like to understand if this notification would serve to get the value in DMA as well.

0 件の賞賛
返信
1,808件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, you can use both.You may specify at which FIFO entry DMA request is triggered.

davidtosenovjan_0-1661858975422.png

 

0 件の賞賛
返信