ADC Data destination - S32K3xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ADC Data destination - S32K3xx

Jump to solution
1,824 Views
MVR
Contributor V

When I define the ADC data destination to FIFO_1, if I'm using DMA, the watermark notification will be notify when the FIFO is full and in this moment the data will be already in the DMA buffer?

Thanks,

MVR

Labels (1)
0 Kudos
Reply
1 Solution
1,786 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, you can use both.You may specify at which FIFO entry DMA request is triggered.

davidtosenovjan_0-1661858975422.png

 

View solution in original post

0 Kudos
Reply
3 Replies
1,816 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Could you please explain your question more in detail? Thanks

0 Kudos
Reply
1,794 Views
MVR
Contributor V

I'm sorry, improving my question:

I would like to understand if it is possible to work FIFO_1 and DMA together or I need to choose only one of both...

Now I'm using only FIFO and all works, there is a notification when finish the ADC conversion, but in the future I will work with DMA, and I would like to understand if this notification would serve to get the value in DMA as well.

0 Kudos
Reply
1,787 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, you can use both.You may specify at which FIFO entry DMA request is triggered.

davidtosenovjan_0-1661858975422.png

 

0 Kudos
Reply