A probably error in S32K SDK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

A probably error in S32K SDK

1,715 次查看
945595199
Contributor I

Hello: 

   I have found a error in the power_smc_hw_access.c in S32_SDK_DFP1.2.0 that in line 363 the register to juge is SMC->PMPROT but the mask bit is PMCTRL, is this a error? ( The Appendix below shows )

   And I have met a application problem: When I allow going to VLPS/HSRUN mode by setting the bits in PMPORT, then go into VLPS mode, but I get a 1 status by reading VLPSA in PMCTRL after wakup by GPIO interrupt. And Only when I make POR reset, the status is correct indicating that I have succeffuly gone into VLPS.

   Thanks! Best Regards!

Appendix:

static bool SMC_CheckVlpsa(const SMC_Type * const baseAddr)
{
bool retValue;
uint32_t regValue = (uint32_t)baseAddr->PMPROT;

regValue = (regValue & SMC_PMCTRL_VLPSA_MASK) >> SMC_PMCTRL_VLPSA_SHIFT;
retValue = (regValue == 0UL) ? false : true;

return retValue;
}

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,603 次查看
945595199
Contributor I

Somebody meet the same confuse?

0 项奖励
回复

1,603 次查看
dianabatrlova
NXP TechSupport
NXP TechSupport

Hello Dan,

You are right, the code is not correct. However, this SW is from Keil MDK. I suggest contacting directly Keil Product Support 

Best regards,

Diana

0 项奖励
回复