H.264 Hardware Encoder support on S32V234

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

H.264 Hardware Encoder support on S32V234

1,586件の閲覧回数
muhammad_nadeem
Contributor I

Hi,

 

We are developing an application to capture videos and want them to encode using H.264 hardware encoder in lossless mode on S32v234. I wonder if the HW H.264 Encode support lossless mode? and where can I find APIs and sample code to utilize hardware encoding. Any pointer will be really appreciated.

-- Muhammad Nadeem

ラベル(1)
0 件の賞賛
返信
1 返信

1,541件の閲覧回数
bpe
NXP Employee
NXP Employee

Please be aware, that support to S32V234 Vision subsystem modules is done only
via tickets. This Community is not appropriate for questions of this kind. I
will contact you by e-Mail with respect to this issue, for future requests,
please use only tickets.

 
Have a great day,
Platon

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信