whether S32DS can generate ‘.abs’ file as same as "codewarrior IDE"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

whether S32DS can generate ‘.abs’ file as same as "codewarrior IDE"

Jump to solution
2,206 Views
jinshuaixu
Contributor V

hello, friends

        l can use "codewarrior IDE" generate '.abs' file ago, now l use s32ds software , l want generate '.abs' file , how to set s32ds software?

        the reason that l want to get '.abs' file is that l want use "vector ASAP2 edit" software to monitor address and variable data.

     thank you.

Labels (1)
Tags (3)
0 Kudos
Reply
1 Solution
2,044 Views
stanish
NXP Employee
NXP Employee

Hi,

The .abs file is in fact an ELF DWARF executable file compliant to elf/dwarf standard file format.

So you can basically rename .elf into .abs if the vector ASAP2 tool does intend on using a specific file extension.

Hope it helps.

Stan

View solution in original post

0 Kudos
Reply
2 Replies
2,045 Views
stanish
NXP Employee
NXP Employee

Hi,

The .abs file is in fact an ELF DWARF executable file compliant to elf/dwarf standard file format.

So you can basically rename .elf into .abs if the vector ASAP2 tool does intend on using a specific file extension.

Hope it helps.

Stan

0 Kudos
Reply
2,044 Views
jinshuaixu
Contributor V

Hi

     Thank you for you response.May you good luck.

0 Kudos
Reply