using lauterbach to program/debug S32G in S32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

using lauterbach to program/debug S32G in S32DS

ソリューションへジャンプ
6,047件の閲覧回数
Rick_Li
NXP Employee
NXP Employee

Hello team,

I'd like to use Lauterbach debugger to program S32G in S32DS v3.4.

the required plug-in for Lauterbach is installed from lauterbach website.

but there are some files missing for S32G debugging. 

see attached image.

Please suggest.

Thank you.

0 件の賞賛
返信
1 解決策
6,036件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @Rick_Li,

If you create a new application project using the wizard, you can select Lauterbach as debugger.

mikedoidge_0-1619107409903.png

Then go to the Debug Configurations menu and you'll find these fields already completed for you. This is done as part of the New Project Wizard. However, when you create a new launch configuration for Lauterbach from within the Debug Configurations, it won't add these details. So you can copy them from the dummy project to the new launch config for the existing project, since they are not project-specific.

mikedoidge_1-1619107809665.png

 

Hope it helps!

Mike

 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
6,037件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello @Rick_Li,

If you create a new application project using the wizard, you can select Lauterbach as debugger.

mikedoidge_0-1619107409903.png

Then go to the Debug Configurations menu and you'll find these fields already completed for you. This is done as part of the New Project Wizard. However, when you create a new launch configuration for Lauterbach from within the Debug Configurations, it won't add these details. So you can copy them from the dummy project to the new launch config for the existing project, since they are not project-specific.

mikedoidge_1-1619107809665.png

 

Hope it helps!

Mike

 

0 件の賞賛
返信