using lauterbach to program/debug S32G in S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

using lauterbach to program/debug S32G in S32DS

Jump to solution
6,071 Views
Rick_Li
NXP Employee
NXP Employee

Hello team,

I'd like to use Lauterbach debugger to program S32G in S32DS v3.4.

the required plug-in for Lauterbach is installed from lauterbach website.

but there are some files missing for S32G debugging. 

see attached image.

Please suggest.

Thank you.

0 Kudos
Reply
1 Solution
6,060 Views
mikedoidge
NXP Employee
NXP Employee

Hello @Rick_Li,

If you create a new application project using the wizard, you can select Lauterbach as debugger.

mikedoidge_0-1619107409903.png

Then go to the Debug Configurations menu and you'll find these fields already completed for you. This is done as part of the New Project Wizard. However, when you create a new launch configuration for Lauterbach from within the Debug Configurations, it won't add these details. So you can copy them from the dummy project to the new launch config for the existing project, since they are not project-specific.

mikedoidge_1-1619107809665.png

 

Hope it helps!

Mike

 

View solution in original post

0 Kudos
Reply
1 Reply
6,061 Views
mikedoidge
NXP Employee
NXP Employee

Hello @Rick_Li,

If you create a new application project using the wizard, you can select Lauterbach as debugger.

mikedoidge_0-1619107409903.png

Then go to the Debug Configurations menu and you'll find these fields already completed for you. This is done as part of the New Project Wizard. However, when you create a new launch configuration for Lauterbach from within the Debug Configurations, it won't add these details. So you can copy them from the dummy project to the new launch config for the existing project, since they are not project-specific.

mikedoidge_1-1619107809665.png

 

Hope it helps!

Mike

 

0 Kudos
Reply