using lauterbach to program/debug S32G in S32DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

using lauterbach to program/debug S32G in S32DS

跳至解决方案
4,596 次查看
Rick_Li
NXP Employee
NXP Employee

Hello team,

I'd like to use Lauterbach debugger to program S32G in S32DS v3.4.

the required plug-in for Lauterbach is installed from lauterbach website.

but there are some files missing for S32G debugging. 

see attached image.

Please suggest.

Thank you.

0 项奖励
回复
1 解答
4,585 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @Rick_Li,

If you create a new application project using the wizard, you can select Lauterbach as debugger.

mikedoidge_0-1619107409903.png

Then go to the Debug Configurations menu and you'll find these fields already completed for you. This is done as part of the New Project Wizard. However, when you create a new launch configuration for Lauterbach from within the Debug Configurations, it won't add these details. So you can copy them from the dummy project to the new launch config for the existing project, since they are not project-specific.

mikedoidge_1-1619107809665.png

 

Hope it helps!

Mike

 

在原帖中查看解决方案

0 项奖励
回复
1 回复
4,586 次查看
mikedoidge
NXP Employee
NXP Employee

Hello @Rick_Li,

If you create a new application project using the wizard, you can select Lauterbach as debugger.

mikedoidge_0-1619107409903.png

Then go to the Debug Configurations menu and you'll find these fields already completed for you. This is done as part of the New Project Wizard. However, when you create a new launch configuration for Lauterbach from within the Debug Configurations, it won't add these details. So you can copy them from the dummy project to the new launch config for the existing project, since they are not project-specific.

mikedoidge_1-1619107809665.png

 

Hope it helps!

Mike

 

0 项奖励
回复