s32 ds debugging problem with KITMPC5744DBEVM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32 ds debugging problem with KITMPC5744DBEVM

1,908件の閲覧回数
elvislin
Contributor I

That is my first time using s32 ds when I debug it always have this problem.  i don't understand what's the mean.

it always run to 61% initializing debugging services and stop.

So how can I solve this problem? thanks a lot! 

no.1.PNG

no1.5.PNG

no.2.PNG

0 件の賞賛
返信
2 返答(返信)

1,804件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi,

This looks like a connection issue between P&E probe and the device.

Please make sure the jtag header is correctly oriented.

You can also experiment with the Delay after reset and communication speed:  https://community.nxp.com/message/934308?commentID=934308#comment-934308 

I'd also recommend you to start with RAM based project - build RAM_Debug build configuration 

pastedImage_1.png

Are you able to connect to the device?

Thanks!

Stan

0 件の賞賛
返信

1,804件の閲覧回数
elvislin
Contributor I

thanks for your response! I ignored that usb voltage was not enough.

0 件の賞賛
返信