s32 design studio change version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32 design studio change version

Jump to solution
2,311 Views
SW_S
Contributor II

hi, nxp team.

I used the s32k144w mcu in s32 design studio for arm (2.2) as an s32k144 project, and then imported the project into s32 design studio for platform (3.5).

I opened the project in s32 design studio for platform, how to change the MCU? (s32k144->s32k144w)

please, ans 

have a nice day.

0 Kudos
Reply
1 Solution
2,282 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @SW_S 

I'm afraid that the most viable option is to generate a new project with the desired part number and copy your application source files from the pre-existing project as well as any customizations you made to the project properties.

Sorry for the inconvenience.

Best Regards, Miguel.

View solution in original post

0 Kudos
Reply
4 Replies
2,279 Views
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @SW_S , 

As @Miguel04 , pointed,

yes S32Design Studio 3.5 does not directly support the switching the processor. You may reuse your user code files and logic accordingly. 

Thank you. Best regards. 

- Mehul Patel

0 Kudos
Reply
2,258 Views
SW_S
Contributor II
Thank you.
0 Kudos
Reply
2,283 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @SW_S 

I'm afraid that the most viable option is to generate a new project with the desired part number and copy your application source files from the pre-existing project as well as any customizations you made to the project properties.

Sorry for the inconvenience.

Best Regards, Miguel.

0 Kudos
Reply
2,260 Views
SW_S
Contributor II
hi,
I expected it.
Something unfortunate has happened that requires me to do it again...
thank you
Have a nice day.
0 Kudos
Reply