s32 cdt headless build issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

s32 cdt headless build issue

2,941 Views
eddy_bts
Contributor III

hi,

I'm using example project, IPCF_Example_multi_instance_S32R45_M7_0

eddy_bts_0-1655352005509.png

There are two issues on headless build.

First, Including path doesn't include in headless build even if all necessary paths are listed as below

eddy_bts_2-1655352324692.png

 

Consequently, All necessary path has to be included in command line as below. Otherwise toochain doesn't find proper header file.

-----------------------------------------------------------------------------------------------------------------------------------------

eclipsec --launcher.suppressErrors -nosplash -data C:\Users\Eddy\workspaceS32DS.3.4 -application org.eclipse.cdt.managedbuilder.core.headlessbuild -build IPCF_Example_multi_instance_S32R45_M7_0/Debug_RAM -import C:\Users\Eddy\workspaceS32DS.3.4\IPCF_Example_multi_instance_S32R45_M7_0 -I C:/NXP/S32DS.3.4/S32DS/software/PlatformSDK_S32XX_2021_12/SW32_RTD_4_4_3_0_0_D2112/Base_TS_T40D11M30I0R0/include -I C:/NXP/S32DS.3.4/S32DS/software/PlatformSDK_S32XX_2021_12/SW32_RTD_4_4_3_0_0_D2112/Base_TS_T40D11M30I0R0/header -I C:/NXP/S32DS.3.4/S32DS/software/PlatformSDK_S32XX_2021_12/SW32_RTD_4_4_3_0_0_D2112/Platform_TS_T40D11M30I0R0/startup/include -I ./RTD/include -I ./IPCF/src/common -I ./IPCF/src/hw -I ./IPCF/src/os -I ./FreeRTOS/Source/include -I ./IPCF/src/hw/s32gen1 -I ./FreeRTOS/Source/portable/GCC/ARM_CM7/r0p1 -I ./generate/include -I ./RTD/include -I ./board -I generate/src

-----------------------------------------------------------------------------------------------------------------------------------------

Second, incremental build doesn't function well. every time I try build in headless, clean build is carried out.

Above two problems don't occur in GUI build.

3 Replies

2,570 Views
AndyCh
Contributor I
I also have the same 2 problems.
0 Kudos
Reply

2,868 Views
eddy_bts
Contributor III

anyone who can answer?

0 Kudos
Reply

2,852 Views
mikedoidge
NXP Employee
NXP Employee

Hello @eddy_bts,

If you use s32ds.exe, instead of eclipse.exe, then it will include the s32ds.ini file.

s32ds.exe -noSplash \

-consoleLog -noExit \

-application com.nxp.swtools.framework.application [tools commands]

If you prefer to use eclipse.exe, then you must include this file manually.

eclipsec.exe -noSplash \

--launcher.ini /path/to/S32DS/installation/eclipse/s32ds.ini

-application com.nxp.swtools.framework.application [tools commands]

 

You can locate more instructions for command line execution from the user documentation inside S32DS. Go to Help -> Help Contents, then S32 Configuration Tools Getting Started -> Command Line Execution

Hope it helps,

Mike

0 Kudos
Reply