s32 _3.4 demo compile error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

s32 _3.4 demo compile error

ソリューションへジャンプ
1,911件の閲覧回数
Lv_Jm
Contributor II
    • When I compile the demo project, the following error occurs.

      • How can I fix this error

    • QQ截图20230427105701.png

0 件の賞賛
返信
1 解決策
1,845件の閲覧回数
Lv_Jm
Contributor II

thanks,A few days ago, I formatted my laptop and reinstalled S32. The problem has been resolved, but thank you all the same.

元の投稿で解決策を見る

4 返答(返信)
1,890件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Lv_Jm 

did you click on Update Code icon in the configuration tool?

This is copied from the example description from user manual:

lukaszadrapa_0-1682573773593.png

 

The button can be found here:

lukaszadrapa_1-1682573858158.png

 

Regards

Lukas

0 件の賞賛
返信
1,884件の閲覧回数
Lv_Jm
Contributor II

I HAVE done that but it still have errors when compiling

0 件の賞賛
返信
1,848件の閲覧回数
mikedoidge
NXP Employee
NXP Employee

Hello,

This error doesn't appear to be the true source of the issue. The incremental build is complaining the object files are not found. Try performing a 'Clean Project' first, then a full build and share the errors that result.

mikedoidge_0-1682951355623.png

Best Regards,

Mike

0 件の賞賛
返信
1,846件の閲覧回数
Lv_Jm
Contributor II

thanks,A few days ago, I formatted my laptop and reinstalled S32. The problem has been resolved, but thank you all the same.