/powerpc-eabivle/bin/real-ld.exe: cannot find -lc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

/powerpc-eabivle/bin/real-ld.exe: cannot find -lc

3,436 Views
InHome
Contributor III

Dear NXP Hello,

I am using the DEVKIT-MPC5748G.

I have a problem when i compile the hello+pll example,

I couldn't compile the project and the console outputs this message:

make -j4 all
Building target: hello+pll_Z2_3.elf
Invoking: Standard S32DS C Linker
"powerpc-eabivle-"gcc -o "hello+pll_Z2_3.elf" "@hello+pll_Z2_3.args"
c:/nxp/s32ds_power_v2.1/s32ds/build_tools/powerpc-eabivle-4_9/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle/bin/real-ld.exe: cannot find -lc
c:/nxp/s32ds_power_v2.1/s32ds/build_tools/powerpc-eabivle-4_9/bin/../lib/gcc/powerpc-eabivle/4.9.4/../../../../powerpc-eabivle/bin/real-ld.exe: cannot find -lm
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:34: hello+pll_Z2_3.elf] Error 1

 

Thank you in advance for your help,

S.Tarik

 

0 Kudos
Reply
1 Reply

2,999 Views
juergenknop
Contributor I

Hello Tarik,

I am currently running into the same Problem when using a Linux console. Have Youor anybody successfully solved that problem?

Best regards

JK

0 Kudos
Reply