lpi2c_master example can't communicate with E2PROM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpi2c_master example can't communicate with E2PROM

1,059 Views
rayray
Contributor I

Hello,

         There is a question that S32K144EVB-Q100/S32 Design Studio for ARM1.3/S32K144 RTM SDK v1.0.0 platform develop communication with E2PROM ,but can't work!

         Connect the J1-3  to Slave SCL and connect the J1-1 to Slave SDA ;Import the example S32K144 RTM SDK v1.0.0 Example Projects/communcation/lpi2c_master and only change the slave adress 0x50,then generate code and build /debug,watch the rusult error, please help!

Thanks

Ray

0 Kudos
Reply
0 Replies