lpi2c_master example can't communicate with E2PROM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

lpi2c_master example can't communicate with E2PROM

1,030件の閲覧回数
rayray
Contributor I

Hello,

         There is a question that S32K144EVB-Q100/S32 Design Studio for ARM1.3/S32K144 RTM SDK v1.0.0 platform develop communication with E2PROM ,but can't work!

         Connect the J1-3  to Slave SCL and connect the J1-1 to Slave SDA ;Import the example S32K144 RTM SDK v1.0.0 Example Projects/communcation/lpi2c_master and only change the slave adress 0x50,then generate code and build /debug,watch the rusult error, please help!

Thanks

Ray

タグ(3)
0 件の賞賛
返信
0 返答(返信)