fatal error: status.h

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

fatal error: status.h

跳至解决方案
1,515 次查看
Hareesh
Contributor II

Hi NXP team,

We are using S32K144 EVK board and S32 design studio v3.5.

We created a simple application project and configured the LPSPI peripheral and generated the code.

However, when I build the project I am getting the following error:

fatal error: status.h: No such file or directory

Please assist me to resolve this issue.

 

Best regards,

Hareesh

0 项奖励
回复
1 解答
1,497 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Hareesh 

I am afraid other customers have reported some irregularities about the support of S32K1 SDK with S32DS v3.5. We recommend using S32DS3.4 for these devices if you are using SDK. 

 

B.R.

VaneB

在原帖中查看解决方案

0 项奖励
回复
2 回复数
966 次查看
mstroven
Contributor III

Can we ever expect an actual solution to this??  At my company it takes an act of God to get IT to approve and install a software package.  Now I have to get them to downgrade me...

0 项奖励
回复
1,498 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Hareesh 

I am afraid other customers have reported some irregularities about the support of S32K1 SDK with S32DS v3.5. We recommend using S32DS3.4 for these devices if you are using SDK. 

 

B.R.

VaneB

0 项奖励
回复