License applicability for S32DS IDE, Compiler toolchain, Libraries

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

License applicability for S32DS IDE, Compiler toolchain, Libraries

2,191 Views
sandeep_kumar_prabhu
Contributor I

For a commercial product, we need to know applicable licensing for following IDE, Compiler Toolchain, Source files, Object files and Libraries:
NXP MICROCONTROLLER USED: SPC5674FF3MVY3

--------------------------------------------------------------------------------------------------------------------
IDE USED: S32 Design Studio for Power Architecture -- Version: 2.1 -- Build id: 190624
--------------------------------------------------------------------------------------------------------------------
COMPILER TOOLCHAIN USED: NXP Embedded GCC for Power Architecture, v4.9.4 build 1705
--------------------------------------------------------------------------------------------------------------------
CONTROLLER SPECIFIC FILES FROM S32DS IDE GENERATED FILES:
flashrchw.c
INTCISRVEC_table.c
intc_sw_handlers.s
MPC56xx__Interrupt_Init.c
Vector.c
startup.S
--------------------------------------------------------------------------------------------------------------------
LIBRARIES USED:
C:/NXP/S32DS_Power_v2.1/S32DS/build_tools/powerpc-eabivle-4_9/bin/../powerpc-eabivle/newlib/lib/e200z7/fp/libc.a
C:/NXP/S32DS_Power_v2.1/S32DS/build_tools/powerpc-eabivle-4_9/bin/../lib/gcc/powerpc-eabivle/4.9.4/e200z7/fp/libgcc.a
--------------------------------------------------------------------------------------------------------------------
OBJECT FILES USED:
C:/NXP/S32DS_Power_v2.1/S32DS/build_tools/powerpc-eabivle-4_9/bin/../lib/gcc/powerpc-eabivle/4.9.4/e200z7/fp/ecrti.o
C:/NXP/S32DS_Power_v2.1/S32DS/build_tools/powerpc-eabivle-4_9/bin/../lib/gcc/powerpc-eabivle/4.9.4/e200z7/fp/ecrtn.o
--------------------------------------------------------------------------------------------------------------------

 

0 Kudos
Reply
1 Reply

1,939 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

S32DS license is in attachment. 

0 Kudos
Reply