failed when debugging ethernet_UDP example project in S32 Design Studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

failed when debugging ethernet_UDP example project in S32 Design Studio

4,010 次查看
yachuanliu
Contributor II

Hello all, a problem occurred when I debug the enet_rmii_udp project in MPC5748G from the S32 Design Studio example. I can’t debug the project successfully. The pictures below are the errors showed in S32 console tab when debugging this project.

 error.PNG

error0.PNGerror1.PNG

Here are some other message you may need.

  1. S32 version: S32 Design Studio for Power Architecture v1.2.
  2. The enet_rmii_udp project: imported from S32DS Example Projects. And I didn’t change anything.捕获.PNG
  3. I debugged the hello example project successfully using the same computer, same MPC5748G.

I really need your help. Thanks.

5 回复数

3,824 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

I tried to reproduce your use case, but unfortunately, I was not successful.

Do you use debug probe or you debug the example using USB and OpenSDA? Could you please send me you debug settings?

Regards,

Martin

3,824 次查看
yachuanliu
Contributor II

Thank you very much for your help. Here are my debug configurations.

捕获.PNG捕获1.PNG捕获2.PNG捕获3.PNG捕获4.PNG捕获5.PNG捕获45.PNG

Regards,

Yachuan

0 项奖励
回复

3,824 次查看
yachuanliu
Contributor II

These are my debug probe and my board. Thank you again for your patience.

IMG_4861.JPG

0 项奖励
回复

3,824 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

thanks for information. Unfortunately, I do not have this debug probe to try it on my side.

Did you try to load all three projects using LaunchGroup or only the one for z4a core?

Could you please try to add 250ms delay after reset?

pastedImage_1.png

Regards,

Martin

3,824 次查看
martin_kovar
NXP Employee
NXP Employee

Hello Yachuan,

which debug probe you use? Also, what is the board you use? Do you have Devkit or MPC5748G Evaluation Board?

Regards,

Martin