errors when closing a project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

errors when closing a project

2,210 Views
bingwang312
Contributor III

I am learning to use S32DS + SDK 3.0.0/3, imported some projects, always got "No source available for "0xxxxxxxxxxxx""  error, and when closing the project, it pops up errors like the picture below, I do not know why. any clue is welcome, thanks

errorclosingproject.pngerrorclosingproject.png

0 Kudos
Reply
2 Replies

2,173 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

what is in "Details  >>" message? 

 

Jiri

0 Kudos
Reply

2,151 Views
bingwang312
Contributor III

hi, Jiri, thanks for your reply. the picture is like below which I would show steps of a SDK PA 3.0.0 example, with some errors pop out:

Opened another example project which uses SDK PA 3.0.0, when start debugging(not play yet), it shows an error as shown in picture below:

bingwang312_0-1638745431877.pngbingwang312_0-1638745431877.png

 

When clicked pause button , it shows another error and the addresses changes when click pause it again and again.

bingwang312_1-1638745432229.pngbingwang312_1-1638745432229.png

 

The picture below shows the debugger console information:

bingwang312_2-1638745432558.pngbingwang312_2-1638745432558.png

 

 

When closing the project, it pops up error , see picture below:

bingwang312_3-1638745432870.pngbingwang312_3-1638745432870.png

 

0 Kudos
Reply