errors when closing a project

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

errors when closing a project

1,661 次查看
bingwang312
Contributor III

I am learning to use S32DS + SDK 3.0.0/3, imported some projects, always got "No source available for "0xxxxxxxxxxxx""  error, and when closing the project, it pops up errors like the picture below, I do not know why. any clue is welcome, thanks

errorclosingproject.png

0 项奖励
回复
2 回复数

1,624 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

what is in "Details  >>" message? 

 

Jiri

0 项奖励
回复

1,602 次查看
bingwang312
Contributor III

hi, Jiri, thanks for your reply. the picture is like below which I would show steps of a SDK PA 3.0.0 example, with some errors pop out:

Opened another example project which uses SDK PA 3.0.0, when start debugging(not play yet), it shows an error as shown in picture below:

bingwang312_0-1638745431877.png

 

When clicked pause button , it shows another error and the addresses changes when click pause it again and again.

bingwang312_1-1638745432229.png

 

The picture below shows the debugger console information:

bingwang312_2-1638745432558.png

 

 

When closing the project, it pops up error , see picture below:

bingwang312_3-1638745432870.png

 

0 项奖励
回复