download separate elf file to microcontroller using S32 Design Studio

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

download separate elf file to microcontroller using S32 Design Studio

1,645 次查看
zengqi300
Contributor II

Background:

    I met trouble during  executing as 

HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio  

steps 。

Console fault message as follows:

“ MPC574xG Device detected.  No breakpoints currently set.  Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "16572" from 7224 Target Disconnected. ”

Whether the elf  os is influential? My  elf file os is MicroSA which from vector。

标记 (2)
0 项奖励
回复
2 回复数

1,548 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share your elf file? If it is compiled for MPC5748G - it should work. 

Jiri 

0 项奖励
回复

1,548 次查看
zengqi300
Contributor II
0 项奖励
回复