download separate elf file to microcontroller using S32 Design Studio

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

download separate elf file to microcontroller using S32 Design Studio

2,190件の閲覧回数
zengqi300
Contributor II

Background:

    I met trouble during  executing as 

HOWTO: download separate elf/srec/hex file to microcontroller using S32 Design Studio  

steps 。

Console fault message as follows:

“ MPC574xG Device detected.  No breakpoints currently set.  Disconnected from "127.0.0.1" via 127.0.0.1. Disconnection by port "16572" from 7224 Target Disconnected. ”

Whether the elf  os is influential? My  elf file os is MicroSA which from vector。

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,093件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

can you please share your elf file? If it is compiled for MPC5748G - it should work. 

Jiri 

0 件の賞賛
返信

2,093件の閲覧回数
zengqi300
Contributor II
0 件の賞賛
返信