custom section in the linker file

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

custom section in the linker file

2,199 Views
oceansea
Contributor III

hi,

now i use S32DS for Power 2.1 IDE ,creat a MPC5748G project .

due to want place some data in a absolute addr ,so i modify the linker file

i add a new section :

/* Define bootFunc SRAM */
BOOTFUNCSRAM_BASE_ADDR = DEFINED(__bootfuncsram_base_addr__) ? __bootfuncsram_base_addr__ : 0x40000000;
 
BOOTFUNCSRAM_SIZE = DEFINED(__bootfuncsram_size__) ? __bootfuncsram_size__ : 4K;
 
m_bootFunc_data : org = BOOTFUNCSRAM_BASE_ADDR,len = BOOTFUNCSRAM_SIZE
 

.BootFuncBlock (NOLOAD):
{
KEEP(*(.BOOTFUNCDATA))
} > m_bootFunc_data

 

but ,when i use this section in .c file   defined  a  struct   

BootDriverFunction     g_BootDriverFunction __attribute__((section (".BOOTFUNCDATA"))) ;

and compile the project ,it show some err:

the target (g_BootDriverFunction) of a R_PPC_VLE_SDA21 relocation is in the wrong output section (.BootFuncBlock)

can you help me?

thankyou!

oceansea

/*
** ###################################################################
**     Processor:           MPC5748G with 256 KB SRAM
**     Compiler:            GNU C Compiler
**
**     Abstract:
**         Linker file for the GNU C Compiler
**
**     Copyright 2017-2019 NXP
**     All rights reserved.
**
**     THIS SOFTWARE IS PROVIDED BY NXP "AS IS" AND ANY EXPRESSED OR
**     IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
**     OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
**     IN NO EVENT SHALL NXP OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT,
**     INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
**     (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
**     SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
**     HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,
**     STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING
**     IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
**     THE POSSIBILITY OF SUCH DAMAGE.
**
**     http:                 www.nxp.com
**
** ###################################################################
*/
 
/* Entry Point */
ENTRY(_start)
 
/* define heap and stack size */
__HEAP_SIZE = DEFINED(__heap_size__) ? __heap_size__ : 0x00000000;
__STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x00001000;
 
/* Define FLASH */
FLASH_BASE_ADDR = DEFINED(__flash_base_addr__) ? __flash_base_addr__ : 0x01000000;
FLASH_SIZE =  DEFINED(__flash_size__) ? __flash_size__ : 1856K;
 
/* Define SRAM */
SRAM_BASE_ADDR = DEFINED(__sram_base_addr__) ? __sram_base_addr__ : 0x40001000;
SRAM_SIZE = DEFINED(__sram_size__) ? __sram_size__ : 252K;
 
/* Define bootFunc SRAM */
BOOTFUNCSRAM_BASE_ADDR = DEFINED(__bootfuncsram_base_addr__) ? __bootfuncsram_base_addr__ : 0x40000000;
BOOTFUNCSRAM_SIZE = DEFINED(__bootfuncsram_size__) ? __bootfuncsram_size__ : 4K;
 
 
/* Define RAppID boot data address */
RAPPID_BOOT_APP_DELAY_ADDR = 0x00FA0008;
RAPPID_BOOT_APP_KEY_ADDR   = 0x00FA000C;
 
MEMORY
{
    flash_rchw : org = 0x00FA0000, len = 0x4
    cpu0_reset_vec : org = 0x00FA0000+0x10, len = 0x4
    cpu1_reset_vec : org = 0x00FA0000+0x14, len = 0x4
    cpu2_reset_vec : org = 0x00FA0000+0x04, len = 0x4
    rappid_boot_data : org = 0x00FA0000+0x08, len = 0x8
 
    m_text : org = FLASH_BASE_ADDR, len = FLASH_SIZE
    m_data : org = SRAM_BASE_ADDR, len = SRAM_SIZE
   m_bootFunc_data : org = BOOTFUNCSRAM_BASE_ADDR,len = BOOTFUNCSRAM_SIZE
}
 
 
SECTIONS
{
    .rchw :
    {
        KEEP(*(.rchw))
    } > flash_rchw
 
    .cpu0_reset_vector :
    {
        KEEP(*(.cpu0_reset_vector))
    } > cpu0_reset_vec
 
    .cpu1_reset_vector :
    {
        KEEP(*(.cpu1_reset_vector))
    } > cpu1_reset_vec
 
    .cpu2_reset_vector :
    {
        KEEP(*(.cpu2_reset_vector))
    } > cpu2_reset_vec
 
    /* RAppID App Delay */
    .RAppID_AppDelay RAPPID_BOOT_APP_DELAY_ADDR :
    {
        KEEP(*(.RAppID_AppDelay))
    } > rappid_boot_data
 
    /* RAppID App Key Address */
    .RAppID_AppKeyAddr RAPPID_BOOT_APP_KEY_ADDR :
    {
        KEEP(*(.RAppID_AppKeyAddr))
    } > rappid_boot_data
 
    /* Note: if you move the 'startup' section shall modify the RCHW2_2 value for the corresponding core in the flashrchw.c file. */
    .startup : ALIGN(0x400)
    {
        __start = .;
        *(.startup)
    } > m_text
 
    .core_exceptions_table : ALIGN(4096)
    {
        __IVPR_VALUE = .;
        *(.core_exceptions_table)
    } > m_text
 
    .intc_vector_table : ALIGN(4096)
    {
        __VECTOR_TABLE = .;
        __interrupts_start__ = .;
        KEEP(*(.intc_vector_table)) /* Startup code */
        __interrupts_end__ = .;
    } > m_text
    __RAM_VECTOR_TABLE_SIZE = 0xC00;
    __VECTOR_TABLE_COPY_END = __VECTOR_TABLE + __RAM_VECTOR_TABLE_SIZE;
 
    .text :
    {
        *(.text.startup)
        *(.text)
        *(.text.*)
        KEEP(*(.init))
        KEEP(*(.fini))
        . = ALIGN(16);
    } > m_text
    .sdata2 :
    {
        . = ALIGN(4);
        __sdata2_start__ = .; /* Create a global symbol at sdata2 start. */
        *(.sdata2)
        *(.sdata2.*)
        . = ALIGN(4);
        __sdata2_end__ = .; /* Define a global symbol at sdata2 end. */
    } > m_text
    .got2 :
    {
        *(.got2*)
    } > m_text
/* migration to version v1.2
   define section PREINIT_ARRAY */
 
.preinit_array :
  {
    PROVIDE_HIDDEN (__preinit_array_start = .);
    KEEP (*(.preinit_array))
    PROVIDE_HIDDEN (__preinit_array_end = .);
  } > m_text
 
/* end section PREINIT_ARRAY */
/*  migration to version v1.2
    define section INIT_ARRAY*/
 
  .init_array :
  {
    PROVIDE_HIDDEN (__init_array_start = .);
    KEEP (*(SORT(.init_array.*)))
    KEEP (*(.init_array ))
    PROVIDE_HIDDEN (__init_array_end = .);
  } > m_text
 
/* end section INIT_ARRAY */
 
/* migration to version v1.2
   define section DTORS */
 
  .dtors :
  {
    KEEP (*crtbegin.o(.dtors))
    KEEP (*crtbegin?.o(.dtors))
    KEEP (*(EXCLUDE_FILE (*crtend.o *crtend?.o ) .dtors))
    KEEP (*(SORT(.dtors.*)))
    KEEP (*(.dtors))
  } > m_text
 
/* end section DTORS */
/* migration to version v1.2
   define section CTORS */
 
  .ctors :
  {
    /* gcc uses crtbegin.o to find the start of
       the constructors, so we make sure it is
       first.  Because this is a wildcard, it
       doesn't matter if the user does not
       actually link against crtbegin.o; the
       linker won't look for a file to match a
       wildcard.  The wildcard also means that it
       doesn't matter which directory crtbegin.o
       is in.  */
    KEEP (*crtbegin.o(.ctors))
    KEEP (*crtbegin?.o(.ctors))
    /* We don't want to include the .ctor section from
       the crtend.o file until after the sorted ctors.
       The .ctor section from the crtend file contains the
       end of ctors marker and it must be last */
    KEEP (*(EXCLUDE_FILE (*crtend.o *crtend?.o ) .ctors))
    KEEP (*(SORT(.ctors.*)))
    KEEP (*(.ctors))
  } > m_text
 
/* end section CTORS */
 
/* migration to version v1.2
   define section FINI_ARRAY */
 
  .fini_array :
  {
    PROVIDE_HIDDEN (__fini_array_start = .);
    KEEP (*(SORT(.fini_array.*)))
    KEEP (*(.fini_array ))
    PROVIDE_HIDDEN (__fini_array_end = .);
  } > m_text
 
/* end  section FINI_ARRAY */
 
    .rodata :
    {
        *(.rodata)
        *(.rodata.*)
    } > m_text
 
    .eh_frame_hdr : { *(.eh_frame_hdr) } > m_text
    .eh_frame : { KEEP (*(.eh_frame)) } > m_text
 
    /* Sections used by startup for data initialization. */
    .init_table :
    {
        . = ALIGN(4);
        __COPY_TABLE = .;
        KEEP(*(.init_table))
    } > m_text
    .zero_table :
    {
        . = ALIGN(4);
        __ZERO_TABLE = .;
        KEEP(*(.zero_table))
    } > m_text
 
    /* RAppID App Key */
    .RAppID_AppKey :
    {
        . = ALIGN(4);
        __RAPPID_APP_KEY_ADDR = .;
        KEEP(*(.RAppID_AppKey))
        . = ALIGN(4);
    } > m_text
 
    __TEXT_END = .; /* Define a global symbol at end of code. */
 
    .interrupts_ram : ALIGN(4096)
    {
        __VECTOR_RAM = .;
        *(.m_interrupts_ram)
        . += __RAM_VECTOR_TABLE_SIZE;
    } > m_data
 
    __CUSTOM_ROM = __TEXT_END; /* Symbol is used by startup for custom initialization. */
    .customSectionBlock : AT (__CUSTOM_ROM)
    {
        . = ALIGN(4);
        __CUSTOM_RAM = .;
        __customSectionStart = .;
        __customSection_start__ = .;
        KEEP(*(.customSection)) /* Keep section even if not referenced. */
        . = ALIGN(4);
        __customSection_end__ = .;
        __customSectionEnd = .;
    } > m_data
    __CUSTOM_END = __CUSTOM_ROM + (__customSection_end__ - __customSection_start__); 
 
    __DATA_ROM = __CUSTOM_END; /* Symbol is used by startup for data initialization. */
    .data : AT (__DATA_ROM)
    {
        . = ALIGN(4);
        __DATA_RAM = .;
        __data_start__ = .; /* Create a global symbol at data start. */
        *(.data)
        *(.data.*)
        . = ALIGN(4);
        __data_end__ = .; /* Define a global symbol at data end. */
    } > m_data
    __DATA_END = __DATA_ROM + (__data_end__ - __data_start__);
 
    __SDATA_ROM = __DATA_END; /* Symbol is used by startup for sdata initialization. */
    .sdata : AT (__SDATA_ROM)
    {
        . = ALIGN(4);
        __SDATA_RAM = .;
        __sdata_start__ = .; /* Create a global symbol at sdata start. */
        *(.sdata)
        *(.sdata.*)
        . = ALIGN(4);
        __sdata_end__ = .; /* Define a global symbol at sdata end. */
    } > m_data
    __SDATA_END = __SDATA_ROM + (__sdata_end__ - __sdata_start__);
 
    .sbss (NOLOAD) :
    {
        . = ALIGN(4);
        __SBSS_START = .;
        __sbss_start__ = .; /* Create a global symbol at sbss start. */
        KEEP(*(.sbss))
        KEEP(*(.sbss.*))
        . = ALIGN(4);
        __sbss_end__ = .; /* Define a global symbol at sbss end. */
        __SBSS_END = .;
    } > m_data
 
    .bss (NOLOAD) :
    {
        . = ALIGN(4);
        __BSS_START = .;
        __bss_start__ = .; /* Create a global symbol at bss start. */
        *(.bss)
        *(.bss.*)
        *(COMMON)
        . = ALIGN(4);
        __bss_end__ = .; /* Define a global symbol at bss end. */
        __BSS_END = .;
    } > m_data
    
    .BootFuncBlock (NOLOAD): 
    {
      KEEP(*(.BOOTFUNCDATA))  
    } > m_bootFunc_data 
    
    __CODE_ROM = __SDATA_END; /* Symbol is used by code initialization. */
    .code : AT (__CODE_ROM)
    {
        . = ALIGN(4);
        __CODE_RAM = .;
        __code_start__ = .; /* Create a global symbol at code start. */
        __code_ram_start__ = .;
        KEEP(*(.code_ram)) /* Custom section for storing code in RAM */
        . = ALIGN(4);
        __code_ram_end__ = .;
        __code_end__ = .; /* Define a global symbol at code end. */
    } > m_data
    __CODE_END = __CODE_ROM + (__code_end__ - __code_start__);
 
    .stack (NOLOAD) : ALIGN(16)
    {
        __HEAP = .;
        PROVIDE (_end = .);
        PROVIDE (end = .);
        . += __HEAP_SIZE;
        __HEAP_END = .;
        _stack_end = .;
        . += __STACK_SIZE;
        . = ALIGN(4);
        _stack_addr = .;
        __SP_INIT = .;
    } > m_data
 
/*-------- LABELS USED IN CODE -------------------------------*/
 
/* Labels Used for Initialising SRAM ECC */
__SRAM_SIZE = SRAM_SIZE;
__SRAM_BASE_ADDR = SRAM_BASE_ADDR;
 
__BSS_SIZE    = __BSS_END - __BSS_START;
 
}

 

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,140 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

you may find helpful this thread - https://community.nxp.com/t5/S32-SDK/Initilization-error-for-Z7a-core/m-p/1322720 

I tested your linker script file with empty project and on my side was testing function properly placed on address 0x40000000 

 

jiri_kral_0-1702909490684.png

 

 

2,107 Views
oceansea
Contributor III

hi,

thank you reply;

now ,i can place the struct in the 0x40000000;

but ,if i write the struct ,the cpu0 will stop.

SRAM_BASE_ADDR = DEFINED(__sram_base_addr__) ? __sram_base_addr__ : 0x40001000;
SRAM_SIZE = DEFINED(__sram_size__) ? __sram_size__ : 252K;

before change the linker file ,the SRAM_SIZE is 256K,

after add a new section ,i change the SRAM_SIZE to 252K,because i hope the cpu0 do not 

Initialise my SRAM(0x40000000~0x40001000).

it seem if the SRAM(0x40000000~0x40001000) have not Initialise ,then the cpu0 will 

disable write these address (0x40000000~0x40001000)

oceansea

 

0 Kudos
Reply