breakpoint installation failed: unmatched quote

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

breakpoint installation failed: unmatched quote

5,188 Views
donliao
Contributor II

I cannot use the breakpoint in S32DS V1.1 and S32DS V1.2, when I set the breakpoint that will be an error message "breakpoint installation failed: unmatched quote".Please help me to solve it, thanks!

Labels (1)
4 Replies

4,856 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please specify, which microcontroller you use and also, what program you have download into the memory?

Regards,

Martin

4,856 Views
donliao
Contributor II

Hi Martin:

I used the S32R274 and downloaded AIPS_cfg(), XBAR_cfg(), PRAMC_cfg(), XOSC_cfg(), PLL0_cfg(), PLL1_cfg(), SDPLL_cfg(), CGM_cfg(), xcptn_xmpl(), etc., thanks!

B.R.

Don

0 Kudos
Reply

4,856 Views
martin_kovar
NXP Employee
NXP Employee

Hello Don,

thanks for information, but I need your project (or at least some test projects which demonstrates your issue) to check it on my side.

Also, which debug probe you use?

Regards,

Martin

4,854 Views
donliao
Contributor II

Hi Martin:

Any projects, for example the S32R274-ModeTransition-S32DS.zip, such as attachment files.

I used the CYCLONE of PEmicro.

Thanks!

B.R.

Don

0 Kudos
Reply