breakpoint installation failed: unmatched quote

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

breakpoint installation failed: unmatched quote

5,186件の閲覧回数
donliao
Contributor II

I cannot use the breakpoint in S32DS V1.1 and S32DS V1.2, when I set the breakpoint that will be an error message "breakpoint installation failed: unmatched quote".Please help me to solve it, thanks!

ラベル(1)
4 返答(返信)

4,854件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

could you please specify, which microcontroller you use and also, what program you have download into the memory?

Regards,

Martin

4,854件の閲覧回数
donliao
Contributor II

Hi Martin:

I used the S32R274 and downloaded AIPS_cfg(), XBAR_cfg(), PRAMC_cfg(), XOSC_cfg(), PLL0_cfg(), PLL1_cfg(), SDPLL_cfg(), CGM_cfg(), xcptn_xmpl(), etc., thanks!

B.R.

Don

0 件の賞賛
返信

4,854件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello Don,

thanks for information, but I need your project (or at least some test projects which demonstrates your issue) to check it on my side.

Also, which debug probe you use?

Regards,

Martin

4,852件の閲覧回数
donliao
Contributor II

Hi Martin:

Any projects, for example the S32R274-ModeTransition-S32DS.zip, such as attachment files.

I used the CYCLONE of PEmicro.

Thanks!

B.R.

Don

0 件の賞賛
返信