about Drag and drop the function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

about Drag and drop the function

1,602 次查看
turbozzg
Contributor II

In s32ds 2008 version, I can drag and drop functions to the main window, but in s32ds 3.3 version, this function is not found。

标签 (1)
0 项奖励
回复
3 回复数

1,589 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi turbozzg,

Please follow the steps in: HOWTO: Working with AMMCLib SDKs

Have you tried "Select the SDK from the list and then click 'Attach/Detach...'"?
Then I am able to achieve it in S32 Design Studio for S32 Platform 3.3.

Drag and drop.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

1,580 次查看
turbozzg
Contributor II

In version 2018, drag in the function to the main window to automatically complete the parameters, but in version 3.3, after dragging in the function, just simply copy the function over, without automatically filling in the parameters

0 项奖励
回复

1,570 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for the inconvenience we bring you!
I am afraid you need to fill these parameters manually.

0 项奖励
回复