about Drag and drop the function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about Drag and drop the function

2,400件の閲覧回数
turbozzg
Contributor II

In s32ds 2008 version, I can drag and drop functions to the main window, but in s32ds 3.3 version, this function is not found。

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,387件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi turbozzg,

Please follow the steps in: HOWTO: Working with AMMCLib SDKs

Have you tried "Select the SDK from the list and then click 'Attach/Detach...'"?
Then I am able to achieve it in S32 Design Studio for S32 Platform 3.3.

Drag and drop.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

2,378件の閲覧回数
turbozzg
Contributor II

In version 2018, drag in the function to the main window to automatically complete the parameters, but in version 3.3, after dragging in the function, just simply copy the function over, without automatically filling in the parameters

0 件の賞賛
返信

2,368件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Sorry for the inconvenience we bring you!
I am afraid you need to fill these parameters manually.

0 件の賞賛
返信