Why the macro of preprocessor is invalid for the newly created configuration?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Why the macro of preprocessor is invalid for the newly created configuration?

ソリューションへジャンプ
2,075件の閲覧回数
liping921
Contributor II

When I create a new configuration based on a configuration, I add a new macro on the new configuration, but this macro is invalid for the new configuration, only adding this macro on the original configuration is valid for the new configuration, what is the reason for this? Isn't it true that the different configurations are not controlled separately?

liping921_1-1701246026770.pngliping921_2-1701246230264.png

 

0 件の賞賛
返信
1 解決策
2,042件の閲覧回数
liping921
Contributor II
Sorry, I didn't notice another problem that I didn't select the corresponding build file after compiling, and now the problem has been solved, only the code is still grayed out, but it doesn't affect the run, thanks for your reply!

元の投稿で解決策を見る

4 返答(返信)
2,031件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi,

in the past there was some issue that preprocessor macros was visible only from First configuration (typically debug_FLASH). What is your S32DS version? Can you try to put this macro definition in first debug configuration and check, if the code is still invalid? 

0 件の賞賛
返信
1,970件の閲覧回数
liping921
Contributor II
Putting the first configuration is valid, our version of S32DS is V
2.2
0 件の賞賛
返信
2,054件の閲覧回数
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @liping921 , 

 

Please can you provide more information to help to understand the issue. 

 

Thank you.  Kind regards. 

- Mehul Patel

0 件の賞賛
返信
2,043件の閲覧回数
liping921
Contributor II
Sorry, I didn't notice another problem that I didn't select the corresponding build file after compiling, and now the problem has been solved, only the code is still grayed out, but it doesn't affect the run, thanks for your reply!